AXIS#.SAFEPARAM.SLS_#.VELLIMIT

Description

Indicates the velocity limit of the Safely Limited Speed (SLS) safety function.

 

D

This value is n_SLS in the following diagram:

Context

For complete SLS information refer to SLS (Safely Limited Speed).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

Depends on user units

Range

[1, 2^31-1]

Default Value

1

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SLS_1.VELLIMIT

315ch

07h

Unsigned32

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLS_2.VELLIMIT

315dh

07h

Unsigned32

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLS_3.VELLIMIT

315eh

07h

Unsigned32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLS_1.VELLIMIT

325ch

07h

Unsigned32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLS_2.VELLIMIT

325dh

07h

Unsigned32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLS_3.VELLIMIT

325eh

07h

Unsigned32

-

-

Read/Write

No